• Menu
  • Product
  • Email
  • PDF
  • Order now
  • How to Reduce Audible Noise in Stepper Motors

    • SLVAES8 May   2020 DRV8424 , DRV8424E , DRV8426 , DRV8428 , DRV8428E , DRV8434 , DRV8434E , DRV8434S , DRV8436 , DRV8436E , DRV8889-Q1

       

  • CONTENTS
  • SEARCH
  • How to Reduce Audible Noise in Stepper Motors
  1.   How to Reduce Audible Noise in Stepper Motors
    1.     Trademarks
    2. 1 Introduction
    3. 2 Details of the Test Setup
    4. 3 Sources of Noise in a Stepper Motor
      1. 3.1 Magnetic Noise
      2. 3.2 Mechanical Noise
      3. 3.3 Electrical Noise
        1. 3.3.1 Effects of Current Ripple and Decay Mode
        2. 3.3.2 Effects of PWM Chopper Frequency
        3. 3.3.3 Effects of Current Zero-cross Error
        4. 3.3.4 Effects of Step Resolution and Step Frequency
        5. 3.3.5 Effects of Resonant Frequency
    5. 4 Summary
    6. 5 References
  2. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

How to Reduce Audible Noise in Stepper Motors

How to Reduce Audible Noise in Stepper Motors

Stepper motors are known to generate audible noise as they operate, which is undesirable for many applications. Traditional stepper motor drivers with fixed-percentage mixed decay current chopping and low levels of microstepping greatly contribute to the noise. But features such as smart tune technology and high microstepping can help lower the audible noise significantly. The goal of this application report is to explain how specific motor driver features can reduce the audible noise for a wide variety of stepper motor systems and applications.

Trademarks

All trademarks are the property of their respective owners.

1 Introduction

Stepper motors are used in a wide array of applications such as printers, projectors, textile machines, stage lighting, industrial automation, electronic point of sale, automotive headlight, and head-up display. A stepper motor moves in discrete steps as defined by a step angle during its rotation. It has two electrical current windings and each winding can be controlled with an H-Bridge. As shown in Figure 1, the stepper motor driver applies current waveforms approximating a sine wave (blue) into one coil and a cosine wave (red) into the other. One quadrant (90°) of the current waveforms corresponds to the stepper motor rotation by one step angle, which is 1.8° for most hybrid stepper motors used today.

microstepping current.jpgFigure 1. Microstepping Current Waveform

Most stepper motor drivers limit current by "chopping" their drive output at some frequency, called the PWM frequency. During PWM current chopping, the H-bridge is enabled to drive through the motor winding until the PWM current chopping threshold is reached. This is shown in Figure 2, Item 1.

Once the chopping current threshold is reached, the H-bridge can operate in two different states, fast decay or slow decay. In fast decay mode, once the PWM chopping current level has been reached, the H-bridge reverses state to allow winding current to flow in a reverse direction. The opposite FETs are turned on; as the winding current approaches zero, the bridge is disabled to prevent any reverse current flow. Fast decay mode is shown in Figure 2, item 2. In slow decay mode, winding current is re-circulated by enabling both of the low-side FETs in the bridge. This is shown in Figure 2, Item 3. Most legacy stepper drivers feature a fixed-percentage mixed decay scheme, where the decay mode is fast decay for a fixed percentage of the OFF time, and slow decay for the rest of the OFF time.

decay.gifFigure 2. Decay Modes

With traditional slow, fast and mixed decay modes, stepper motors can be known to hum and whine as they operate. In most applications, the audible noise can annoy users and might warrant expensive noise suppression methods, such as rubber isolators, which do not completely eliminate the noise. For example, household or office printers and 3D printers have multiple stepper motors within them, and the noise from the motors can break concentration of their users. Higher quality stepper motor drivers that can reduce the motor noise go a long way towards user satisfaction. Another example is electric vehicles, which are generally quiet due to the absence of an internal combustion engine, and lowering the noise level from stepper motors used in headlight leveling helps to achieve a overall quiet cabin.

In the following sections, we will discuss the various sources of noise in stepper motors and how different stepper motor driver features can alleviate most of that noise.

2 Details of the Test Setup

In this application report, several measurements were taken to demonstrate the effectiveness of different settings in stepper motor drivers in reducing the motor noise. Sound pressure level (SPL) was used as one method of measurement. SPL is the measurement of local pressure deviation from the ambient pressure caused by a sound wave. SPL is represented graphically with sound in decibels (dB) versus frequency. To obtain the SPL plots shown in this application report, a microphone and a stepper motor driven by a DRV8424 driver were placed inside an acoustic chamber. The audible noise from the stepper motor was recorded at various operating conditions to obtain SPL plots. Figure 3 shows a picture of the microphone inside the chamber. The details of the setup are as follows:

  • The motor was securely mounted on rubber to minimize extra vibrations.
  • The stepper motor is rated for 2.3 A, has 1.8° step angle, 1.9 mH inductance and 0.93 Ω resistance.
  • A calibrated USB microphone was used for recording the noise.
  • First, a few seconds ( approximately 5 sec) of ambient noise was captured to use as reference.
  • Then, a few seconds (approximately 5-10 secs) of audio was recorded while the motor was spinning.
  • The files from the audio recording were imported to a software to obtain the SPL plots.
Test setup.jpgFigure 3. Audible Noise Measurement Setup

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale