• Menu
  • Product
  • Email
  • PDF
  • Order now
  • LMR54410EVM User's Guide

    • SLUUCK7 October   2021 LMR54410

       

  • CONTENTS
  • SEARCH
  • LMR54410EVM User's Guide
  1.   Trademarks
  2. 1Introduction
  3. 2Setup
    1. 2.1 Input/Output Connector Description
    2. 2.2 Adjusting the Output Voltage
  4. 3 LMR54410EVM Schematic
  5. 4Board Layout
  6. 5Bill of Materials
  7. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

USER'S GUIDE

LMR54410EVM User's Guide

Trademarks

All trademarks are the property of their respective owners.

1 Introduction

The Texas Instruments LMR54410EVMevaluation module (EVM) helps designers evaluate the operation and performance of the LMR54410 wide-input buck regulator.

GUID-20210930-SS0I-WTNV-SRWB-ZKFJWKDCXTZS-low.pngFigure 1-1 LMR54410EVM Board

EVM Features

  • 4-V to 36-V input voltage range
  • Default 3.3-V output
  • Up to 1-A output current
  • 1100-kHz switching frequency
  • Hiccup mode short current protection
  • Internal compensation

The EVM contains one DC/DC converter (see Table 1-1).

Table 1-1 Device and Package Configurations
CONVERTEREVMDEVICEPACKAGE
U1LMR54410EVMLMR54410SOT23-6

2 Setup

This section describes the jumpers and connectors on the EVM and how to properly connect, set up, and use the LMR54410EVM.

2.1 Input/Output Connector Description

VIN — Terminal TP1 – Power input terminal for the converter. Adjacent to it is the GND reference ground. Use this terminal to attach the EVM to a cable harness.

VOUT — Terminal TP3 – Regulated output voltage for the converter. Adjacent to it is the GND reference ground.

GND — Terminal TP2, TP4 – Ground reference for the converter. Use these terminals to attach the EVM to a cable harness.

ENABLE SETTING — Jumper JP1 – Used to enable the switch-mode converter. The device will be enabled when the EN pin is high, and disabled when low.

GUID-9BB98B12-0CF6-4338-87EF-ABA334FC5EB4-low.gifFigure 2-1 Enable Jumper Setting

Testpoint — TP7, TP6, TP9 – Test points used for loop response measurements

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale