• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Designing a Simple and Low-Cost Flybuck Solution With the TPS62933F

    • SLUAAN0 December   2022 TPS62933F

       

  • CONTENTS
  • SEARCH
  • Designing a Simple and Low-Cost Flybuck Solution With the TPS62933F
  1.   Designing a Simple and Low-Cost Flybuck Solution With the TPS62933F
  2.   Trademarks
  3. 1Introduction
  4. 2Flybuck Converter Device Overview
    1. 2.1 Operation Description
    2. 2.2 Equations for Maximum Output Current
  5. 3Design Flybuck With TPS62933F
    1. 3.1 Primary Voltage and Turns Ratio
    2. 3.2 Feedback Resistor
    3. 3.3 Rectifier Diode
    4. 3.4 Primary Inductance
    5. 3.5 Primary Turns
    6. 3.6 Input and Output Capacitor
    7. 3.7 Pre-Load
    8. 3.8 Factors Affecting Voltage Regulation
    9. 3.9 Avoiding Low-Side Sink Current Limit
  6. 4Experimental Results
  7. 5Conclusion
  8. 6References
  9. IMPORTANT NOTICE
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
APPLICATION NOTE

Designing a Simple and Low-Cost Flybuck Solution With the TPS62933F

1 Designing a Simple and Low-Cost Flybuck Solution With the TPS62933F

In many applications, simple, low part-count, isolated power supplies working from an input voltage are needed. A popular solution to these requirements is an isolated buck power supply. This application report presents a simple and low-cost flybuck solution using the TPS62933F device. The basic operating principles of a flybuck converter are discussed, operating current and voltage waveforms are shown, and key design equations are derived. Lastly, a step-by-step design example is presented.

Trademarks

All trademarks are the property of their respective owners.

1 Introduction

Isolated bias rails are common in many systems or subsystems, such as telecommunication equipment, medical equipment, and industrial factory automation. It is mandatory by safety standards to protect users from the hazardous voltage of a power supply, or the isolation is installed to break the ground loop interference for noise-sensitive applications.

In many cases, simple, low part count, isolated power supplies working from an input voltage are needed. This design solution is for when regulation may not be as important, but cost and board area are. A popular solution to these requirements is an isolated buck power supply, which is a synchronous buck converter, with the inductor replaced by a coupled inductor or flyback-type transformer. There is no need for an optocoupler or auxiliary winding because the secondary output closely tracks the primary voltage, resulting in smaller solution size and cost. The flybuck can support a simple, small, and cost effective power solution making it suitable as a flyback alternative.

This application report presents the basic operating principles of a flybuck converter, shows some typical operating current and voltage waveforms, and the key design equations are derived. The design example shows a step-by-step procedure for designing one nonisolated and two isolated outputs with the synchronous buck regulator TPS62933F.

The TPS62933F device is a 3.8-V to 30-V input voltage range, 3-A switching regulator, that has two integrated switching FETs and internal loop compensation. By integrating the MOSFETs and employing the SOT-5x3 package, the TPS63933F achieves high-power density and offers a small footprint on the PCB.

2 Flybuck Converter Device Overview

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale