• Menu
  • Product
  • Email
  • PDF
  • Order now
  • DRV8662, DRV2700, DRV2665, and DRV2667 Configuration Guide

    • SLOA198A September   2014  – December 2021 DRV2665 , DRV2667 , DRV2700 , DRV8662

       

  • CONTENTS
  • SEARCH
  • DRV8662, DRV2700, DRV2665, and DRV2667 Configuration Guide
  1.   Trademarks
  2. 1 Boost Converter Basics
  3. 2 DRV8662, DRV2700, DRV2665, and DRV2667 Boost Converter
    1. 2.1 DRV8662, DRV2700, DRV2665, and DRV2667 Boost Converter Efficiency
      1. 2.1.1 Boost Efficiency vs Boost Current
    2. 2.2 DRV8662, DRV2700, DRV2665, and DRV2667 Boost Converter Load Regulation
      1. 2.2.1 Boost Regulation vs Current
  4. 3 Configuring the Boost Converter
  5. 4 Boost Converter Output Voltage
  6. 5 Calculating the Load Current
  7. 6 Selecting an Inductor
    1. 6.1 Inductance Rating
    2. 6.2 Saturation Current Rating
    3. 6.3 Thermal Current Rating
    4. 6.4 Choosing REXT
    5. 6.5 What to Avoid: Using Incorrect Inductor Current Ratings
  8. 7 Calculate the Maximum Boost Current
  9. 8 Output Capacitor Selection
  10. 9 Input Capacitor Selection
  11. 10PCB Layout
    1. 10.1 What to Avoid: Incorrect Inductor Placement
  12. 11Examples
    1. 11.1 Example: Based on the DRV8662EVM
      1. 11.1.1 Configure the Boost Voltage
      2. 11.1.2 Configure the Inductor Current
      3. 11.1.3 Boost Performance Results
    2. 11.2 Example: Based on the DRV2667EVM-CT with 25-nF Piezo Module
      1. 11.2.1 Configure the Boost Voltage
      2. 11.2.2 Configure the Inductor Current
      3. 11.2.3 Boost Performance Results
  13. 12Revision History
  14. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

DRV8662, DRV2700, DRV2665, and DRV2667 Configuration Guide

Trademarks

All trademarks are the property of their respective owners.

1 Boost Converter Basics

A boost converter, as the name implies, converts a low voltage power rail and boosts it to a higher voltage. A boost converter consists of three main components: an inductor, a switch (MOSFET), and a diode. The basic boost converter schematic is shown in the following figure.

GUID-2B5C40A2-CE41-4FFF-9143-16FAEE4A522F-low.gif

To convert the low voltage to a high voltage, the boost converter operates in two phases. In the first phase the inductor is charged by closing the switch and forcing current through the inductor to ground. During this period the current through the inductor increases allowing the inductor to store charge.

GUID-E28DE3E3-FF89-45FA-B014-2AB4F0EA899F-low.gif

Once the inductor current reaches a maximum threshold, the switch opens and forces the inductor to dump the stored charge through the diode and onto the output capacitor and load.

GUID-61257F54-4E41-4EB6-83A6-B02F1E4FC163-low.gif

By repeating this charge and dump process, the boost converter is able to increase the output voltage.

2 DRV8662, DRV2700, DRV2665, and DRV2667 Boost Converter

The DRV8662, DRV2700, DRV2665, and DRV2667 use a hysteretic boost converter design to generate the high voltage needed to drive Piezos. This section describes the basic operating principle of the hysteretic boost converter.

The hysteretic boost converter uses fairly simple feedback to control the timing and frequency of the switch. The ILIM value in the following figure is the peak current through the inductor every time the switch turns on. Once the peak current is reached, the switch opens. The peak inductor current of the DRV8662, DRV2665, and DRV2667 is set by the resistor on the REXT pin (pin 15).

GUID-134AACAB-AAFA-484F-A821-A2FC7D07C0CE-low.gif

The boost converter only switches when the output voltage (VBST) is below the final target value, meaning that it will only switch when it needs to. Unlike a fixed-frequency boost converter design, the hysteretic boost converter design has a continually varying switching frequency and is load-dependent. Note that the DRV8662, DRV2665, and DRV2667 have forced switching at approximately 37 kHz.

2.1 DRV8662, DRV2700, DRV2665, and DRV2667 Boost Converter Efficiency

The boost converter efficiency for the DRV8662, DRV2700, DRV2665, and DRV2667 is shown in Figure 2-1 through Figure 2-4. The measurements were taken using the DRV8662EVM.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale