• Menu
  • Product
  • Email
  • PDF
  • Order now
  • TPSM82821, TPSM82822, TPSM82823, TPSM82821A, TPSM82822A, and TPSM82823APin Failure Mode Analysis (Pin FMA)

    • SFFS293 September   2021 TPSM82821 , TPSM82821A , TPSM82822 , TPSM82822A , TPSM82823 , TPSM82823A

       

  • CONTENTS
  • SEARCH
  • TPSM82821, TPSM82822, TPSM82823, TPSM82821A, TPSM82822A, and TPSM82823APin Failure Mode Analysis (Pin FMA)
  1.   Trademarks
  2. 1Overview
  3. 2Pin Failure Mode Analysis (Pin FMA)
  4. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

FUNCTIONAL SAFETY FIT RATE, FMD AND PIN-FMA

TPSM82821, TPSM82822, TPSM82823, TPSM82821A, TPSM82822A, and TPSM82823APin Failure Mode Analysis (Pin FMA)

Trademarks

All trademarks are the property of their respective owners.

1 Overview

This document contains the Pin failure mode analysis (pin FMA) information for the TPSM82821, TPSM82822, TPSM82823, TPSM82821A, TPSM82822A, and TPSM82823A (uSiP package).

Figure 1-1 shows the device functional block diagram for reference.

GUID-20211117-SS0I-D0PW-8F4D-DBMPPDRJSQGZ-low.jpgFigure 1-1 Functional Block Diagram

The TPSM8282x was developed using a quality-managed development process, but was not developed in accordance with the IEC 61508 or ISO 26262 standards.

2 Pin Failure Mode Analysis (Pin FMA)

This section provides a failure mode analysis (FMA) for the pins of the TPSM8282x. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

  • Pin short-circuited to ground (see Table 2-2)
  • Pin open-circuited (see Table 2-3)
  • Pin short-circuited to an adjacent pin (see Table 2-4)
  • Pin short-circuited to VIN (see Table 2-5)

Table 2-2 through Table 2-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 2-1.

Table 2-1 TI Classification of Failure Effects
ClassFailure Effects
APotential device damage that affects functionality.
BNo device damage, but loss of functionality.
CNo device damage, but performance degradation.
DNo device damage, no impact to functionality or performance.

Figure 2-1 shows the TPSM8282x pin diagram. For a detailed description of the device pins, see the Pin Configuration and Functions section in the TPSM8282x data sheet.

GUID-20211117-SS0I-MHR5-WGPQ-W3V3BKLVW7SC-low.jpg Figure 2-1 Pin Diagram

Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:

  • The device is operating in the typical application, please refer to the Simplified Application on the first page in the TPSM8282x datasheet.
Table 2-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class

VIN

1,2

Device will not be powered up

A

EN

3

Device will not be enabled

B

PG

4

Loss of PG functionality

B

VOUT

5,6,7

Device not functional

A

FB

8

Output voltage will not be regulated. Device will enter 100% mode.

B

GND

9,10

Intended functionality

D

Table 2-3 Pin FMA for Device Pins Open-Circuited
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class

VIN

1,2

Redundant pin. If one of the pins are open, no functionality loss but potential impact on device performance

C

EN

3

Undetermined state of the pin; device may or may not be enabled

B

PG

4

Loss of PG functionality

B

VOUT

5,6,7

Redundant pin. If one of the pins are open, no functionality loss but potential impact on device performance

C

FB

8

Device not functional; Open loop operation

B

GND

9,10

Redundant pin. If one of the pins are open, no functionality loss but potential impact on device performance

C

Table 2-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin NamePin No.Shorted toPin No.Description of Potential Failure Effect(s)Failure Effect Class

VIN

2

EN

3

Loss of Enable functionality

B

EN

3

PG

4

Loss of Enable functionality; Potential device damage

A

PG

4

VOUT

5

Loss of PG functionality; Potential device damage

A

VOUT

7

FB

8

For adjustable versions output voltage will be regulated to 0.6V (Intended functionality for Fixed Vout devices)

B

FB

8

GND

9

Output voltage will not be regulated. Device will enter 100% mode.

B

Table 2-5 Pin FMA for Device Pins Short-Circuited to VIN
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class

VIN

1

Intended functionality

D

EN

3

Loss of Enable functionality

B

PG

4

Loss of PG functionality; Potential device damage

A

VOUT

5,6,7

Potential device damage

A

FB

8

Device not functional; Open loop operation

B

GND

9,10

Potential device damage

A

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale