• Menu
  • Product
  • Email
  • PDF
  • Order now
  • TMUX7208EVM Evaluation Module

    • SCDU018A December   2020  – December 2020 TMUX7208

       

  • CONTENTS
  • SEARCH
  • TMUX7208EVM Evaluation Module
  1.   Abstract
  2.   Trademarks
  3. 1 Introduction
  4. 2 Information About Cautions and Warnings
  5. 3 Features of this EVM
  6. 4 EVM Images
  7. 5 EVM Setup
  8. 6 EVM Connectors and Test Points
    1. 6.1 Connectors
    2. 6.2 Test Points
  9. 7 PCB Layouts
  10. 8 Schematics
  11. 9 Bill of Materials
  12. 10Related Documentation
  13. 11Revision History
  14. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

USER'S GUIDE

TMUX7208EVM Evaluation Module

Abstract

This user's guide describes the characteristics, operation, and use of the TMUX7208EVM evaluation module (EVM). A complete schematic diagram, printed-circuit board layouts, and bill of materials are included in this document.

Trademarks

All trademarks are the property of their respective owners.

1 Introduction

The TMUX7208EVM supports evaluation of the TMUX7208 device in the 16-pin TSSOP (PW) package. TMUX7208 is a complementary metal-oxide semiconductor (CMOS) switch with latch-up immunity in a 8:1 single channel configuration. The device supports dual supplies (±4.5 V to ±22 V), a single supply (4.5 V to 44 V), or asymmetric supplies (such as VDD = 12 V, VSS = –5 V). The TMUX7208 supports bidirectional analog and digital signals on the source (Sx) and drain (D) pins ranging from VSS to VDD. All logic control inputs support logic levels from 1.8 V to VDD, ensuring both TTL and CMOS logic compatibility when operating in the valid supply voltage range. The Fail-Safe Logic circuitry applies voltages on the control pins before the supply pin, which protects the device from potential damage.

2 Information About Cautions and Warnings

GUID-7937F995-C8AE-47DA-B3F1-B4E3B2B67E94-low.png
CAUTION: This EVM contains components that can potentially be damaged by electrostatic discharge. Always transport and store the EVM in its supplied ESD bag when not in use. Handle using an antistatic wristband. Operate on an antistatic work surface. For more information on proper handling, see Electrostatic Discharge (ESD) application report

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale