• Menu
  • Product
  • Email
  • PDF
  • Order now
  • How to Handle High Voltage Common Mode Applications using Multiplexers

    • SCDA043 October   2022 MUX36D08 , TMUX6136 , TMUX6208 , TMUX6219 , TMUX6219-Q1 , TMUX6234 , TMUX6236 , TMUX7208 , TMUX7219 , TMUX7219-Q1 , TMUX7234 , TMUX7236 , TMUX7308F , TMUX7309F , TMUX7348F , TMUX7349F , TMUX8108 , TMUX8109 , TMUX8212

       

  • CONTENTS
  • SEARCH
  • How to Handle High Voltage Common Mode Applications using Multiplexers
  1.   Abstract
  2.   Trademarks
  3. 1Differential, Single-Ended, and Common Mode Signals
  4. 2Characteristics of Interest for Selecting a Multiplexer for High Voltage Common Mode Applications
    1. 2.1 Operating Supply Range
    2. 2.2 Crosstalk and Bandwidth
    3. 2.3 Leakage Current
    4. 2.4 Fault Protection
  5. 3Multiplexers in High Voltage Common Mode Applications
    1. 3.1 PLC Multi-Channel Analog I/O Modules
    2. 3.2 CAN Bus Multiplexing Applications with High Voltage Common Mode
    3. 3.3 High Voltage Battery Cell Monitoring
  6. 4Recommended Multiplexers for High Voltage Common Mode Applications
  7. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

How to Handle High Voltage Common Mode Applications using Multiplexers

1 Abstract

High common mode voltages can often be a top concern when designing in a particularly noisy or harsh environment as they can cause irreparable damage to a signal chain or significantly impact a system's accuracy. However, sometimes high common mode voltages are present by design and the overall system needs to be able to accommodate these high voltages for everything to cohesively work together. Whether intentional or not, the components along the signal chain need to be able to withstand and operate effectively in these conditions and TI’s multiplexer portfolio offers many options to handle a myriad of situations where this can be a possibility while also offering the performance needed for any application. In this report, several high common mode voltage applications will be explored which will include analog I/O modules for programmable logic controllers, industrial protocols such as CAN or RS485, and battery cell monitoring.

Trademarks

All trademarks are the property of their respective owners.

1 Differential, Single-Ended, and Common Mode Signals

Differential signals are standard for many different communications protocols including LVDS, CAN, USB, RS485/422, HDMI, and so on and incorporates two complementary signals (differential pair) that are used to transmit data.

Figure 1-1 Differential vs. Single-Ended Signals

While single ended communication protocols such as I2C or SPI are often more ubiquitous due to their simplicity and are referenced to a single, stationary potential, differential signaling offers numerous advantages over single ended communication schemes and several are as follows:

  • EMI (electromagnetic interference) and Common Mode Noise Resistance
  • EMI and Common Mode Noise can be introduced from a variety of sources that can be coupled to the data transmission signals and can distort what the receiver is reading. In protocols with differential signaling, this effect is mitigated significantly as the noise is emitted onto both signals meaning that each inverted and non-inverted signal will constructively cancel each other out once they reach the receiver:
Figure 1-2 EMI Resistance in Differential Signals
  • Ground Shift Immunity
  • In addition, many differential signal protocols do not share any common ground or return current path, so ground reference shifts and ground noise acquired along the path are of no concern when utilizing such differential signaling protocols. However, for protocols that do call for common termination (such as the CAN interface as an example), there needs to be more care taken to reduce ground offsets as much as possible.
  • Reduced Power Requirements and Higher Frequency Operation
  • Differential signaling often calls for voltage signals to be in the hundreds of millivolts or just up to 1 V or 2 V and can greatly simplify power consumption needs of an application. In turn, this also allows these differential signals to operate at higher frequencies due to the much lower radiated emissions these signals have from the smaller voltages used (in addition to the resistance from external EMI imposed by using a differential pair).

Common mode signals can be simply defined as the voltage that is common between the input terminals of a device and are often an unwanted element in most systems. For instance, take the visual representation as shown in Figure 1-3.

Figure 1-3 Common Mode Voltage

It is evident that when a common mode voltage is introduced to a system, this will shift the reference point of the affected components to be outside of the anticipated operating range by a given VCM (as shown above from both a graphical and equivalent circuit perspective). While common mode signals can be attributed to EMI, ground shifts, miswirings, coupling, or even lightning strikes, they can be influential enough to the system at large that it can significantly affect measurement accuracy or even permanently damage devices by causing them to exceed absolute maximum operating ratings. Hence, it is essential that the design is defined by the environment the system will be used in and components selected that can tolerate such conditions.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale