• Menu
  • Product
  • Email
  • PDF
  • Order now
  • OPA928 Evaluation Module

    • SBOU282A December   2022  – March 2023 OPA928

       

  • CONTENTS
  • SEARCH
  • OPA928 Evaluation Module
  1.   Abstract
  2.   Trademarks
  3. 1Read This First
    1. 1.1 EVM Cleanliness Guidelines
  4. 2Overview
    1. 2.1 Guarding and Shielding
  5. 3Getting Started
    1. 3.1 Related Documentation From Texas Instruments
    2. 3.2 Electrostatic Discharge Caution
  6. 4EVM Circuit Description
    1. 4.1 High-Impedance Amplifier Circuit
    2. 4.2 Transimpedance Amplifier Circuit
      1. 4.2.1 Configure the TIA
      2. 4.2.2 TIA Functions
        1. 4.2.2.1 T-Switch
        2. 4.2.2.2 Guarded Diode Limiter
  7. 5Cleaning the EVM
    1. 5.1 Ultrasonic Wash
    2. 5.2 Manual Cleaning Procedure
  8. 6Schematic, PCB Layout, and Bill of Materials
    1. 6.1 EVM Schematic
    2. 6.2 PCB Layout
    3. 6.3 Bill of Materials
  9. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

EVM USER'S GUIDE

OPA928 Evaluation Module

Abstract

GUID-20221209-SS0I-STMJ-30Z8-KRXZQS87RN0K-low.jpg

This user’s guide describes the operation and use of the OPA928 evaluation module (EVM). The user's guide provides information on how to set up the EVM and describes different circuit configurations that can be used to evaluate the performance of the OPA928 femtoampere, input-bias-current op amp. Throughout this document, the terms evaluation board, evaluation module, and EVM are synonymous with the OPA928EVM. This document also includes an electrical schematic, simplified schematics of OPA928 applications circuits, a printed circuit board (PCB) layout drawing, and a parts list for the EVM.

Note: For best possible performance, make sure to review the Section 1.1 before handling the EVM board.

Trademarks

All trademarks are the property of their respective owners.

1 Read This First

1.1 EVM Cleanliness Guidelines

Applications requiring femtoampere-level performance are extremely sensitive to contamination. Contaminants in the form of solder flux, salts, oils, organic acids, and more can form conductive paths over PCB traces that allow small currents to leak into input traces or other sensitive nodes, thus degrading performance. For best possible performance, make sure to keep the OPA928EVM as clean as possible.

The following list of best practices helps prevent the EVM from becoming contaminated:

  • Always wear a fresh, clean pair of powder-free gloves or finger cots when handling the OPA928EVM.
  • When handling the EVM, always hold the board by the edges.
  • Avoid touching the surface of the PCB, especially near sensitive nodes or input traces.
  • Be cautious when breathing, speaking, sneezing, and so on, to prevent moisture or saliva from contacting the EVM.
  • Do not allow direct airflow from cooling fans or ionizers onto the board. Moving air can blow dust and moisture onto sensitive nodes. Additionally, airflow introduces moving charges that present as a small current at the input.
  • When not in use, place the EVM in ESD bag or other enclosure to prevent dust and other contaminants from settling on the board.
  • When configuring through-hole components in the TIA feedback path, handle the components by the wire leads only. Avoid touching the component package.

The OPA928EVM undergoes a rigorous cleaning protocol before shipping to customers, providing femtoampere-level performance directly out of the box. Follow the cleaning procedures detailed in Section 5 to maintain best performance. The EVM must be cleaned per these instructions anytime the board is soldered or modified near sensitive nodes, or if these nodes become contaminated by other means.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale