Bidirectional Current Sense Amplifiers (CSA) are capable of measuring current flowing in either direction. The quiescent output level corresponds to zero current. One, sometimes two output reference pins are available for configuring the zero current voltage. A bidirectional CSA can function in unidirectional mode by setting the quiescent output at or close to either of the supply rails. There are many ways of driving the reference pins. The most common methods include using a reference IC, a voltage divider, or a voltage divider followed by a buffer. Output impedance of the driving source impacts the CSA output and may cause significant error if not designed properly. A voltage divider has the advantage of being versatile and inexpensive. It also tends to occupy less area. As a result, it finds adoption in many applications.
All trademarks are the property of their respective owners.
One way to classify a Current Sense Amplifier (CSA) is based on whether it is able to measure current in both directions. Then it can be put into one of two categories - unidirectional or bidirectional. A unidirectional device only linearly responds to current flowing in one direction, with its output moving in one direction in proportion to the input differential signal. A current flowing in the opposite direction causes the output to collapse to one of the supply rails, normally ground. Figure 1-1 illustrates such a scenario.
For a bidirectional CSA, current flowing in either direction is allowed. The output of the device moves off of a quiescent output level, in proportion to the input differential signal. The fact that bidirectional CSA output is able to move up toward supply or down toward ground implies that the quiescent output level corresponds to zero current. In these devices, there is typically one or two output reference pins. The output is level-shifted by driving the reference pins with a suitable source. Figure 1-2 shows the same bidirectional input is accurately reproduced. A bidirectional CSA can be configured as unidirectional by setting the quiescent output at or close to either supply rail.
This report reviews TI’s bidirectional CSA then examines different ways of configuring the output reference, associated performance tradeoffs, and the reasons behind these tradeoffs. Next, the impact of the resistor divider driving reference pins in common CSA architectures is explored. The goal is to help designers make an informed decision when choosing a reference driving circuit that meets performance requirements, and is economical at the same time.