• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Super-beta Input Amplifiers: Features and Benefits

    • SBOA305 October   2020 INA828 , OPA210 , OPA2210

       

  • CONTENTS
  • SEARCH
  • Super-beta Input Amplifiers: Features and Benefits
  1. 1Application Brief
  2. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content
APPLICATION BRIEF

Super-beta Input Amplifiers: Features and Benefits

1 Application Brief

Introduction

Texas Instruments (TI) new generation of bipolar amplifiers are built on a precision complementary bipolar semiconductor technology that incorporates super-beta bipolar transistors. Super-beta transistors are optimized for high current gain (β > 1000) which helps reduce the device’s input bias current and input bias current drift over temperature.

This technology also incorporates advancements leading to better transistor matching and temperature stability yielding higher precision. This tech note will explain how super-beta transistors improve precision performance in bipolar amplifiers.

What is super-beta?

The beta (β) of a transistor, or transistor current gain, is the ratio of the transistor’s collector current (Ic) to its base current (Ib), as shown in Equation 1.

Equation 1. β = Ic/Ib

The β value is fixed for a given transistor and operating condition. Figure 1 shows a simplified amplifier input stage using bipolar transistors.

GUID-20200921-CA0I-2DSW-0LN1-Z2TG6ZNN2KZT-low.gifFigure 1-1 Simplified differential amplifier input stage

The value of β for traditional bipolar transistors typically ranges from 50 to 200 which may lead to a sizeable base current for a given collector current. For example, a transistor with a β value of 100 and Ic of 10 μA will require 100 nA of Ib.

In contrast, transistors with super-beta technology have a much higher β value, often well over 1000, greatly reducing the Ib needed for a given Ic. Revisiting the example above, for a transistor with a β value of 1000, the required Ib is decreased to only 10 nA. This is a 10x improvement over traditional bipolar transistors

Why do we care about base current?

In an amplifier, base current of the input transistors translates to input bias current (IB). Traditional bipolar amplifiers offer better speed-to-power ratio and lower noise, however, they tend to suffer from higher IB when compared to other silicon technologies like CMOS. The higher IB may be unsuitable for high source impedance applications.

While CMOS and JFET amplifiers offer a clear advantage on IB, new super-beta bipolar amplifiers offer significantly lower IB while still providing the same benefits as the traditional process (speed-to-power ratio, lower voltage noise, lower 1/f noise, and lower open loop output impedance). To learn more about bipolar process advantages take look at the Trade-offs Between CMOS, JFET, and Bipolar Input Stage Technology application report.

What are the benefits of lower IB?

Lower IB translates to lower input current noise. The relationship between IB and current noise is best described by Equation 2. The current noise (in) of a bipolar amplifier is given by

Equation 2. in = √2*q*IB

where q is the elementary charge (1.6 x 10-19 C). It follows that the lower IB of a super-beta amplifier results in lower current noise.

In addition, lower IB translates to higher input resistance (rin). The small signal relationship between IB and rin is given by Equation 3.

Equation 3. rin = β/gm = Ic/Ib * VT/Ic = VT/IB

Where gm is the transconductance and VT is the thermal voltage (equal to about 25 mV at 25⁰C). Equation 3 can be simplified to show the inverse relationship between rin and IB. It follows that the lower IB of a super-beta amplifier will result in higher rin.

System level noise benefits

Unlike DC offset which can be calibrated out, filtering noise is not a trivial task. In applications with high source impedance, in translates to high input voltage noise density (en). For example, 2 pA/√Hz of in typically found in traditional bipolar amplifiers may seem acceptable. However, with a 1 MΩ source impedance the in translates to 2 μV/√Hz of en, which may be inadequate for many applications. On the other hand, a super-beta amplifier like the OPA2205 and OPA2206 with an in of 200 fA/√Hz yields 0.2 μV/√Hz. An order of magnitude improvement.

A traditional bipolar amplifier with ultra-low noise of 1 nV/√Hz with the in from the example above in a 10 kHz filter bandwidth and a circuit gain of 10 yields 350 μVrms of total noise (en + in). In contrast, a super-beta amplifier like OPA2205 with a higher noise floor (7.2 nV/√Hz) results in 41 μVrms under the same conditions, an 8.5x improvement.

Applications such as medical instrumentation, life sciences, and vibration sensing often require the use of high resolution analog-to-digital converters (ADCs) at rather low frequencies. Super-beta amplifiers such as TI's OPA2210 with low 1/f noise (90 nVpp) and OPA2202 with an ultra-low 1/f noise corner (0.1 Hz) help reduce total errors at the output of the amplifier interfacing the ADC.

How about a comparison?

Texas Instruments offers an extensive portfolio of precision bipolar devices. Table 1-1 compares the INA118, an instrumentation amplifier with traditional bipolar transistors, to the INA818, a precision instrumentation amplifier with super-beta transistors. Thanks to the super-beta inputs of INA818 the current noise is reduced by a factor of almost 20, and IB is reduced by a factor of about 10.

A new level of precision with super-beta

In addition to a reduction in IB and in, TI’s super-beta technology results in better transistor matching and better temperature stability, yielding higher precision. Improved DC precision specifications include lower input offset voltage and offset voltage drift over temperature. Table 1-2 shows a comparison between two high voltage precision operational amplifiers: the OPA2209, with traditional bipolar transistor input stage and the OPA2210, with super-beta transistor input stage. These devices both have the same pinout and functionality, but OPA2210 has improved specifications due to the implementation of super-beta technology.

Where can I get a super-beta amplifier?

Table 1-3 highlights some of TI’s precision amplifiers with super-beta technology. For a full list, see our parametric search tool results by visiting ti.com/amps

Table 1-1 Super-beta vs. traditional bipolar instrumentation amplifiers

Device

Attribute

IB (nA)

in (pApp)

INA818 (super-beta)

Typical

0.15

4.7

Maximum

0.50

-

INA118 (traditional)

Typical

1.00

80.0

Maximum

5.00

-

Table 1-2 Super-beta vs. traditional bipolar op amps

Device

Attribute

IB (nA)

in (fA/√Hz)

Zin (Ω)

Vos (μV)

Vos Drift (μV/°C)

OPA2210 (super-beta)

Typical

0.3

400

400

5

0.1

Maximum

2.0

-

-

35

0.6

OPA2209 (traditional)

Typical

1.0

500

200

35

1.0

Maximum

4.5

-

-

150

-

Table 1-3 Super-beta devices

Super-beta devices

Description

THP210 (3 V to 36 V)

Industry's first high voltage fully-differential, low noise (3.7 nV/√Hz) amplifier and ADC driver.

INA848 (8 V to 36 V)

Ultra-low noise (1.3 n/√Hz), high speed (45V/μs, 2.8 MHz), high precision amplifier with fixed gain of 2000.

INA818 (4.5 V to 36 V)

Low power (350 μA), high precision (35 μV), low noise instrumentation amp with over-voltage protection (gain pins 1, 8).

INA819 (4.5 V to 36 V) Low power (350 μA), high precision (35 μV), low noise instrumentation amp with over-voltage protection (gain pins 2, 3). Now available in 3 mm x 3 mm QFN package.

INA821 (4.5 V to 36 V)

Wide bandwidth (4.7 MHz), low noise (7 nV/√Hz), high precision (35 μV) instrumentation amp with over-voltage protection. Now available in 3 mm x 3 mm QFN package.

OPA1637 (3 V to 36 V)

Fully differential, Burr-Brown™ Audio amp with low noise easily filters and drives fully differential audio signal chains.

OPA2210 (4.5 V to 36 V)

Ultra-low noise (2.2 nV/√Hz), high precision (35 μV), wide bandwidth amplifier (18 MHz).

OPA2205 (4.5 V to 36 V)

High precision (25 μV), low power (250 μA), low noise, e-TrimTM amplifier.

OPA2202 (4.5 V to 36 V)

High capacitive drive (25 nF), ultra-low 1/f noise corner (0.1 Hz), precision, dual amplifier.

OPA207 (4.5 V to 36 V)

Precision, low noise amp replaces industry standard OP-07, OP-77, and OP-177 with higher speed (1 MHz) and lower power (375 μA).

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2020, Texas Instruments Incorporated
Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale