• Menu
  • Product
  • Email
  • PDF
  • Order now
  • TMAG5253EVM User's Guide

    • SBAU400 November   2023 TMAG5253

       

  • CONTENTS
  • SEARCH
  • TMAG5253EVM User's Guide
  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Overview
    1. 1.1 Kit Contents
    2. 1.2 Related Documentation From Texas Instruments
  5. 2Hardware
    1. 2.1 Features
  6. 3Operation
    1. 3.1 Quick Start Setup
    2. 3.2 EVM Operation
  7. 4Schematics, PCB Layout, and Bill of Materials
    1. 4.1 Schematic
    2. 4.2 Component Functions
    3. 4.3 PCB Layout
    4. 4.4 Bill of Materials
  8. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

User's Guide

TMAG5253EVM User's Guide

Abstract

This user’s guide describes the characteristics, operation, and use of the TMAG5253 evaluation module (EVM). This EVM is designed to evaluate the performance of the TMAG5253. Throughout this document, the terms evaluation board, evaluation module, and EVM are synonymous with the TMAG5253EVM. This document includes a schematic, reference printed circuit board (PCB) layouts, and a complete bill of materials (BOM).

Trademarks

All trademarks are the property of their respective owners.

1 Overview

The TMAG5253 is a low-power, linear Hall effect sensor with an enable pin. This device is available in multiple unipolar or bipolar sensitivity range variants. The enable pin allows the user to activate a < 10-nA sleep mode, and the fast start-up feature of the device allows the user to duty cycle the enable pin to lower the average power consumption.

Table 1-1 TMAG5253 Device Summary
PRODUCTSENSITIVITY RANGE
TMAG5253BA1IQDMRR100 mV/mT, ±21-mT Range

1.1 Kit Contents

Table 1-2 lists the contents of the EVM kit. Contact the nearest Texas Instruments Product Information Center if any component is missing.

Table 1-2 Kit Contents
ITEMQUANTITY
TMAG5253EVM1
3D printed Trigger Assembly1
Magnet1

Figure 1-1 shows the 3D printed Trigger Assembly with a trigger top, trigger base, torsion spring, and an aluminum axle rod.

GUID-20220901-SS0I-KRQP-S2WL-K9JVFHSN0GD1-low.svgFigure 1-1 Trigger Assembly Exploded View

1.2 Related Documentation From Texas Instruments

This user's guide is available from the TI website under literature number SBAU400. Any letter appended to the literature number corresponds to the document revision that is current at the time of the writing of this document. Newer revisions are available from www.ti.com or the Texas Instruments' Literature Response Center at (800) 477-8924 or the Product Information Center at (972) 644-5580. When ordering, identify the document by both title and literature number. Table 1-3 lists the documentation related to the EVM. Click the links in Table 1-3 for further information. The device name links to the product web folder on www.ti.com. The literature number links to the document PDF.

Table 1-3 Related Documentation

DOCUMENT TITLE

DOCUMENT LITERATURE NUMBER

TMAG5253 data sheet SBASAI5

2 Hardware

This EVM allows the user to evaluate the TMAG5253. The EVM includes a trigger attachment that controls the perceived brightness of an onboard RGB LED according to the analog output of the TMAG5253. The EVM is intended to provide basic functional evaluation of the devices. The layout is not intended to be a model for the target circuit, nor is it laid out for electromagnetic compatibility (EMC) testing.

2.1 Features

  1. LED indicator for visual feedback corresponding to an analog output.
  2. Receptacle for a CR-10-25 Coin Cell Battery to power the EVM.
  3. 3D CAD files available for modifying and customizing trigger design.

3 Operation

3.1 Quick Start Setup

The following instructions describe how to set up and use the EVM.

  1. Supply power to the device through one of these methods:
    • Apply a 3.3-V potential (see Figure 3-1)
    • Insert a CR1025 coin cell battery into the holder (see Figure 3-1)
  2. Toggle the enable switch on.
GUID-20220906-SS0I-4BBX-WP13-RWHTCXKK5TRX-low.svgFigure 3-1 Powering On EVM
GUID-20220906-SS0I-WKLD-67L2-KJGPL4HBXSQL-low.svgFigure 3-2 Enable TMAG5253

3.2 EVM Operation

While the TMAG5253 is available in either unipolar or bipolar configurations, the device featured in this EVM is a bipolar ratiometric device. The device output is an analog signal proportional to the field detected by the sensor. The output is routed to a header pin as well as a via which a test point or wire can be inserted into for inspection with an external voltmeter, oscilloscope, or microcontroller. The output is also routed to an onboard microcontroller that processes the analog potential and generates a PWM signal that can dim an RGB LED indicator to provide visual feedback to the user. If no LED light is on, the device is either disabled or there is little to no field measured. As in Figure 3-3, a bright red LED light indicates that the north pole is facing the top of the device sensing element, while a bright blue LED light, as in Figure 3-4, indicates that the south pole is facing the top of the device sensing element. When the board is inserted into the 3D attachment with the magnet installed, a little less than 50% of the analog output range will be observed over the trigger's range of motion according to the magnetic polarity facing the device.

GUID-20231004-SS0I-NQKN-ZNZJ-V9VVWKGVH7NZ-low.pngFigure 3-3 Red LED Operation
GUID-20231004-SS0I-B3JL-GNK1-WFNLTK6ZLQCD-low.pngFigure 3-4 Blue LED Operation

4 Schematics, PCB Layout, and Bill of Materials

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale