• Menu
  • Product
  • Email
  • PDF
  • Order now
  • BOOSTXL-ADS7142-Q1 BoosterPack™ Plug-In Module

    • SBAU321B November   2018  – June 2021 ADS7142 , ADS7142-Q1

       

  • CONTENTS
  • SEARCH
  • BOOSTXL-ADS7142-Q1 BoosterPack™ Plug-In Module
  1.   Trademarks
  2. 1Introduction
  3. 2BOOSTXL-ADS7142-Q1 EVM Overview
    1. 2.1 Connectors for Single-Ended Analog Input
    2. 2.2 Digital Interface
    3. 2.3 ADS7142-Q1 Digital I/O Interface
    4. 2.4 Power Supplies
  4. 3BOOSTXL-ADS7142-Q1 EVM Initial Setup
    1. 3.1 Running ADS7142-Q1 GUI Online and TI Cloud Agent Application Installation
    2. 3.2 Hardware Setup Instructions
    3. 3.3 ADS7142-Q1 GUI Description
      1. 3.3.1 Description
      2. 3.3.2 REGMAP
      3. 3.3.3 Functional Mode
      4. 3.3.4 General Instructions
  5. 4ADS7142-Q1 GUI Functional Modes
    1. 4.1 Autonomous Mode
      1. 4.1.1 Start Burst Mode
      2. 4.1.2 Stop Burst Mode
      3. 4.1.3 Pre Alert Mode
      4. 4.1.4 Post Alert Mode
    2. 4.2 High Precision Mode
    3. 4.3 Manual Mode
      1. 4.3.1 Default Mode
      2. 4.3.2 Auto Mode
    4. 4.4 Temperature Monitoring Using BOOSTXL-ADS7142-Q1
    5. 4.5 Input Signal Conditioning Block on the BOOSTXL-ADS7142-Q1
  6. 5Bill of Materials, Printed-Circuit Board Layout, and Schematics
    1. 5.1 Bill of Materials
    2. 5.2 PCB Layout
    3. 5.3 Schematics
  7. 6Revision History
  8. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

USER'S GUIDE

BOOSTXL-ADS7142-Q1 BoosterPack™ Plug-In Module

Trademarks

BoosterPack is a trademark of Texas Instruments Incorporated.

is a trademark of Texas Instruments.

Firefox is a trademark of Mozilla Foundation.

Chrome is a trademark of Google LLC..

All trademarks are the property of their respective owners.

1 Introduction

The ADS7142-Q1 BoosterPack™ is a fully-assembled evaluation platform designed to highlight the ADS7142-Q1 features and various modes of operations that makes this device suitable for ultra-low-power, small-size sensor monitor applications.

The accompanying Precision ADC Motherboard (PAMB) development kit is used as a USB-to-PC GUI communication bridge, and example implementation of a master MCU to communicate with the ADS7142-Q1 through its I2C interface.

Note:

The BOOSTXL-ADS7142-Q1 requires an external master controller to evaluate the ADS7142-Q1.

The PAMB is controlled by commands received from the ADS7142-Q1 GUI, and returns data to the GUI for display and analysis. If the PAMB is not used, the BoosterPack™ plug-in module format of the BOOSTXL-ADS7142-Q1 board allows an alternative external host to communicate with the ADS7142-Q1.

The BOOSTXL-ADS7142-Q1 incorporates all required circuitry and components with the following features:

  • ADS7142-Q1 nano power, ultra-small, dual-channel sensor monitor with I2C interface and alert output
  • Optional low power voltage reference, TI’s REF3133-Q1, to generate a 3.3-V output to power the ADS7142-Q1 AVDD supply pin when the 5-V USB power from the PAMB
  • Optional adjustable linear regulator, TI’s TPS79933-Q1, to generate stable output voltage to power the ADS7142-Q1 DVDD pin when using the 5-V USB power from the PAMB
  • I2C interface for communication and configuration of modes available on the ADS7142-Q1

Figure 1-1 shows the ADS7142-Q1EVM architecture, identifying the key components and blocks previously listed.

GUID-B5F6E311-4BD8-4622-98B7-08892785FAA5-low.gifFigure 1-1 ADS7142-Q1 EVM Block Diagram

2 BOOSTXL-ADS7142-Q1 EVM Overview

This section describes various onboard components that are used to interface analog input, digital interface, and provide power supply to BOOSTXL-ADS7142-Q1. Figure 2-1 shows a BOOSTXL-ADS7142-Q1 overview.

GUID-3B927D57-8FC1-4DC6-9F2A-38412B42759D-low.png Figure 2-1 BOOSTXL-ADS7142-Q1 Top Level Overview

2.1 Connectors for Single-Ended Analog Input

The BOOSTXL-ADS7142-Q1 is designed for easy interface to an external, analog, single-ended source through a 100-mil header. Connector J5 allows analog source connectivity. Table 2-1 lists the analog input connector and input channel configuration.

Table 2-1 Input Connector and Channel Configuration
J5 Connector Pin Description
J5:1 Single-ended analog input for channel 0 of ADC
J5:2 Single-ended analog input for channel 1 of ADC
J5:3 and J5:4 BoosterPack™ ground

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale