{"words":[["0","[音乐播放]"],["3030","大家好，欢迎观看"],["3850","TI"],["4670","高精度实验室视频。"],["5490","本视频将讨论"],["6510","I2C"],["7530","总线的规格以及"],["8550","在选择支持"],["9735","该协议的开关时"],["10920","需要注意的事项。"],["12720","在本视频中，"],["13485","我们将讨论"],["14250","I2C"],["15015","的"],["15780","标准总线规格、"],["17900","总线电容、开漏结构"],["20020","和上拉电阻。"],["23120","首先我们将"],["23840","讨论"],["24560","I2C"],["25280","协议的"],["26000","规格，"],["27890","然后学习"],["29010","什么是总线电容，"],["30130","什么是开漏结构，"],["32180","以及为什么"],["33500","需要上拉电阻。"],["34820","本视频的目标"],["35910","是让您了解"],["37000","I2C"],["38090","总线协议的"],["39590","规格、开漏结构，"],["41090","并能根据一些因素，"],["42620","如导通电阻、导通电容"],["44150","和电流限制，"],["46930","选择适合的信号开关。"],["51000","本视频假设大家"],["51795","对"],["52590","I2C"],["53385","通信协议"],["54180","有了基本的了解。"],["55685","如需了解更多"],["56433","关于"],["57182","I2C"],["57931","的基础知识，"],["58680","请观看"],["59560","training.ti.com"],["60440","上的系列视频，或者查阅"],["61320","应用手册"],["63960","“了解"],["65076","I2C"],["66193","总线”。"],["67310","在为"],["68037","I2C"],["68765","应用选择"],["69492","适合的信号开关时，"],["70220","一定要考虑"],["71370","I2C"],["72520","协议的"],["73670","规格。"],["75097","视频中的三种"],["76138","双向传输速率，"],["77180","即标准模式、"],["80000","快速模式和"],["81665","超快速模式，"],["83330","时钟速度分别是"],["84485","100Kbps、400Kbps"],["85640","和"],["86630","1Mbps，"],["87620","每种速率都有"],["88610","不同的规格。"],["90050","所示表格描述了"],["90675","每个"],["91300","I2C"],["91925","协议规格中"],["92550","SDA"],["93268","和"],["93986","SCL"],["94704","信号的"],["95422","最大允许上升时间、"],["96140","每个总线线路的"],["98255","容性负载以及"],["100370","低电平输出电压。"],["101930","请注意，随着"],["103040","数据传输速率的增加，"],["104150","上升时间会大大缩短。"],["106130","在标准模式下，"],["107349","上升时间为"],["108569","1,000ns，"],["109789","而在超快速模式下，"],["112700","上升时间为"],["113690","120ns，"],["114680","几乎缩短了"],["115720","8"],["116760","倍。"],["117800","在获取"],["118530","I2C"],["119260","协议规格时，"],["119990","一定要考虑"],["122960","所有寄生电容的来源。"],["125120","电容的来源包括"],["126290","主设备的电容"],["127460","Cmaster，"],["128630","每个"],["129473","从设备的电容"],["130316","Cslave，"],["131160","以及"],["132140","PCB"],["133120","导线的电容"],["134100","Cpcb。"],["135080","所有这些电容相加"],["135856","得出总线的总电容"],["136633","Cbus，"],["137410","也就是"],["138263","Cbus"],["139116","="],["139970","Cmaster"],["140577","+"],["141184","Cslave"],["141791","+"],["142398","Cpcb。"],["146234","每增加一个从设备，"],["146979","SDA"],["147724","和"],["148469","SCL"],["149214","信号线的"],["149960","总线电容将成比例地"],["152310","增加。"],["153620","每增加一个从设备，Cbus"],["156260","就会增加数十法拉。"],["158120","最终，总线电容将大到"],["160200","无法再按照"],["160839","I2C"],["161478","协议规格"],["162117","支持更多的从设备。"],["165890","有个简单的方法"],["166625","可以解决这个问题，"],["167360","那就是使用"],["168050","多对"],["168740","SDA/SCL"],["169430","总线，"],["170120","由主设备进行复用。"],["172945","这样，主设备就能与"],["174320","更多的"],["175220","从设备进行通信，"],["176120","因为总线电容"],["177425","Cbus"],["178730","被分配到了"],["179832","多对"],["180935","SDA/SCL"],["182037","线上。"],["183140","请注意，多路复用器的"],["184440","开关单元含有导通电阻"],["185740","Ron"],["186880","和导通电容"],["188020","Con。"],["189160","这两个值都会"],["189897","影响总"],["190635","RC"],["191372","常数，"],["192110","进而影响"],["193000","I2C"],["193890","协议规格中的"],["194780","上升时间。"],["196690","这种设计方案"],["197830","虽然允许增加"],["198970","许多从设备，"],["200114","但会因选择的"],["201258","信号开关受到"],["203050","很大影响。"],["205150","比如，有一个"],["206185","低导通电阻的开关，"],["207220","其导通电阻为"],["208705","0.26Ω，"],["210190","导通电容为"],["211825","250pF。"],["213460","还有一个"],["214660","低导通电容的开关，"],["215860","其导通电阻为"],["217247","5.7Ω，"],["218635","导通电容为"],["220022","1.4pF。"],["221410","第一个信号开关"],["222775","虽然导通电阻比"],["224140","第二个开关小，"],["226120","但导通电容"],["227755","约为第二个开关的"],["229390","178"],["230200","倍。"],["231010","请记住，在标准"],["232405","模式传输速率下，"],["233800","总线电容"],["235053","不能超过"],["236306","400pF。"],["237560","低导通电阻开关的电容"],["238650","已占了规格的一半以上，"],["239740","总线能增加的"],["241405","从设备数量就受到了"],["243070","限制。"],["244905","而第二个开关由于"],["246092","其低导通电容的特性，"],["247280","能够支持添加"],["249135","更多的从设备。"],["250990","要了解影响"],["251700","I2C"],["252410","协议规格的其他因素，"],["253120","需要讨论"],["253742","在"],["254365","I2C"],["254987","主从设备中"],["255610","常见的"],["256630","GPIO"],["257650","引脚"],["258670","开漏结构和"],["260605","输入缓冲器"],["262540","结构。"],["264190","左边展示的是"],["265150","带有开漏结构和"],["266110","输入缓冲器结构的"],["267955","主设备或从设备。"],["269800","请注意，"],["270820","当[不可听清]打开时，"],["271840","GPIO"],["272869","引脚的"],["273898","输出会被拉到地。"],["274927","而当[不可听清]关闭时，"],["276760","GPIO"],["278340","引脚的输出会悬空。"],["279920","引脚悬空会导致"],["281220","设备出现意外的"],["282520","电气行为。"],["283600","由于引脚未连接，"],["285370","会起到"],["286435","微型天线的作用，"],["287500","接收电磁和热噪声。"],["289960","要解决引脚悬空问题，"],["290492","在"],["291025","VDD"],["291557","上连接一个"],["292090","上拉电阻即可。"],["294550","连接后，"],["295570","当[不可听清]关闭时，"],["296590","GPIO"],["297570","引脚的输出"],["298550","一定会被上拉到"],["299530","VDD。"],["300510","添加上拉电阻是为了"],["302290","消除电源接地短路，"],["304450","帮助将信号"],["305583","拉高到逻辑"],["306716","1。"],["307850","这个上拉电阻"],["308710","RPU"],["309570","直接增加了"],["310430","RC"],["310808","时间常数，"],["311186","影响了"],["311564","I2C"],["311942","协议"],["312320","规格中的上升时间。"],["316415","从前面的"],["317727","例子中可以看出，"],["319040","由于添加了信号开关，"],["322020","上拉电阻将"],["323287","通过总线的总电容，"],["324555","即"],["325353","Cbus"],["326152","+"],["326951","Con，接地。"],["327750","这个"],["328325","RC"],["328900","时间常数"],["329475","会影响每个总线的"],["330050","上升时间。"],["332970","在为"],["333797","I2C"],["334625","应用选择"],["335452","恰当的信号开关时，"],["336280","一定要考虑上拉电阻的"],["338710","最小值和最大值。"],["340540","请注意，"],["341300","最小上拉电阻"],["342060","Rp(min)"],["342820","是电源电压"],["343757","VCC、"],["344695","低电平输出电压"],["345632","VOL"],["346570","和低电平"],["347605","输出电流"],["348640","IOL"],["349675","的函数。"],["350710","信号开关的"],["351790","绝对最大范围"],["352870","必须能够支持"],["354010","电源电压和电流"],["355150","规格。"],["357700","请注意，"],["358520","最大上拉电阻"],["359340","Rp(max)"],["360160","是上升时间"],["361010","tr"],["361860","和"],["362710","总线总电容"],["363560","Cb"],["364410","的函数。"],["365260","在选择信号开关时，"],["366385","开关的导通电容将"],["367510","直接影响这个计算值。"],["370720","总之，在选择"],["371297","适用于"],["371875","I2C"],["372452","协议"],["373030","应用的单个开关时，"],["374830","有四个关键特性需要"],["376630","考虑。"],["379050","1."],["379900","电源电压必须"],["380750","符合开关的绝对最大"],["381600","额定值。"],["383700","电源电压还会影响"],["385290","允许的最大上拉电阻，"],["386880","从而直接影响总线的"],["388950","上升时间。"],["391140","2."],["391800","开关电流"],["392460","I-switch"],["393120","必须符合开关的"],["394860","绝对最大电流额定值"],["397040","3."],["398243","每个信号开关都有"],["399446","一定的导通状态电阻，"],["400650","会通过"],["401195","RC"],["401740","时间常数"],["402285","直接增加总线的上升"],["402830","时间。"],["404980","4."],["405833","必须考虑"],["406686","开关的导通状态电容，"],["407540","因为这个值会"],["408057","极大地影响"],["408575","I2C"],["409092","协议"],["409610","规格中的总线电容"],["411710","和上升时间规格。"],["415909","导通状态电容"],["416794","还将限制总线"],["417680","可以支持的"],["419240","从设备数量。"],["423090","要了解有关"],["424035","上拉电阻及其计算的"],["424980","更多详细信息，"],["426780","请立即查看此应用。"],["428580","可以在"],["429270","ti.com"],["429960","上的"],["430650","开关/多路复用器类别下"],["431340","搜索我们的模拟开关"],["433635","和多路复用器目录。"],["435930","可使用快速搜索"],["437340","引擎，找到合适的开关。"],["438750","可以按配置、"],["440145","通道数量进行筛选，"],["441540","也可以使用“特性”"],["442830","选项卡上的下拉箭头，"],["444120","为您的"],["445482","I2C"],["446845","应用"],["448207","查找合适的信号开关。"],["449570","本视频介绍了"],["450696","I2C"],["451823","协议规格，"],["452950","以及在为"],["453500","I2C"],["454050","应用"],["454600","选择合适的信号开关时"],["457659","要考虑的参数。"],["459070","请观看下一个视频，了解"],["460020","I2C"],["460970","特定应用中多路复用器的"],["461920","常见用例。"]],"paragraphs":[0,3030],"speakers":{}}